AXIS#.PL.ERRWTHRESH
Description
If this value is not equal 0 and the position error AXIS#.PL.ERR is larger than this value, the drive will generate a warning.
If AXIS#.PL.ERRWTHRESH is set to 0 the warning is not issued.
Example
Set position rotary units to 2 degrees. If you set AXIS#.PL.ERRWTHRESH to 100 and the position error is larger than 100 degrees, then the drive will generate a warning.
AXIS#.UNIT.PROTARY 2
AXIS#.PL.ERRWTHRESH 100
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
0 counts |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.PL.ERRWTHRESH | 0x500C | 0x2 | DINT | - | Position | RW | False |
| AXIS2.PL.ERRWTHRESH | 0x510C | 0x2 | DINT | - | Position | RW | False |
|
Copyright © 2018 Kollmorgen |
|